Part one: User basics - Johnson Controls - LIT-12012230 - Nurses Station Display - NSD1380 Nurses Station Display

NSD1380 Nurses Station Display Technical Bulletin

Product
Accessories > Nurses Station > NSD1380 Nurses Station Display
Document type
Technical Bulletin
Document number
LIT-12012230
Revision date
2021-03-29

This section provides a brief overview of the NSD1380 Nurses Station Display. These few pages explain the purpose and the operation of the display. Technical product information is available in Part two: Technical section .