Passcode - Johnson Controls - LIT-12012230 - Nurses Station Display - NSD1380 Nurses Station Display

NSD1380 Nurses Station Display Technical Bulletin

Product
Accessories > Nurses Station > NSD1380 Nurses Station Display
Document type
Technical Bulletin
Document number
LIT-12012230
Revision date
2021-03-29

NSD1380 Nurses Station Display has passcodes to limit unauthorized access to the room mode or complete menu system. The access codes can be turned on or off through the Passcode menu item. When the display ships from the factory, it is configured with the access code on. See Configuration for instructions on entering the access code.