Meters tab - Johnson Controls - LIT-12012585 - Software Application - JEM: Johnson Controls Enterprise Management - 1.3.1

Metasys Enterprise Management Professional Productivity Tool (PPT) Guide

Product
Building Automation Systems > Building Automation Systems > Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Version
1.3.1
Revision date
2018-12-11

If the project creation process finds meter points, those points display in the Meters tab.

The discovery process uses factors such as units of measure and common naming conventions to identify meters in the System Configuration Tool archive data. Select the Meters tab to enable the Meter Wizard feature, which limits the display to meter types and is a more convenient method for you to create meter equipment from the points in the Meters tab. For more information about the Meter Wizard, see Using the Meter Wizard feature. You can select a different Data Source tab to return the Equipment tabs to their original view. You can also use the two Assessment View options under the View menu to return to the original Equipment tab view.