Installing the Professional Productivity Tool - Johnson Controls - LIT-12012585 - Software Application - JEM: Johnson Controls Enterprise Management - 1.3.1

Metasys Enterprise Management Professional Productivity Tool (PPT) Guide

Product
Building Automation Systems > Building Automation Systems > Johnson Controls Enterprise Management
Document number
LIT-12012585
Version
1.3.1
Revision date
2018-12-11

About this task

You can install the Professional Productivity Tool when your computer complies with the system requirements.

For more details about the installation process and requirements, see Additional and operational considerations.

Complete the following steps to install the Professional Productivity Tool:

Procedure

  1. Download the Professional Productivity Tool install package from the Johnson Controls® SharePoint site and save it to your Downloads folder.
  2. Right-click on the file PPTInstaller64-1.2.0.zip.
  3. Click Open.
  4. Drag the PPTInstaller64-1.2.0.msi folder onto the desktop.
  5. Right-click on the PPTInstaller64-1.2.0.msi folder.
  6. Click Install and follow the installation wizard instructions.
    A notification displays confirmation of a successful installation when the installation is complete.
  7. Navigate to C:\ProgramData\Johnson Controls\Third Party Installs.
  8. Run VisualBasicPowerPacksSetup.exe and follow the installation wizard instructions to install the VB power pack.
    Note: You do not need to complete this step for a subsequent PPT upgrade.
    Note: We recommend that you create a desktop shortcut to start PPT, and another desktop shortcut to access the PPT data folder.
    • The full path to the executable file is: C:\Program Files (x86)\Johnson Controls\PPT for Metasys Enterprise Management (MEM)\ProfessionalProductivityTools.exe.
    • The full path to the PPT data folder is: C:\ProgramData\Johnson Controls\PPT.