About this task
You can identify points that do not have the correct unit of measure or enumeration type for their point type requirements in Johnson Controls. To identify these points, you can check the units and enumeration from the Action menu. In some cases, the units of measure are incorrect in the Johnson Controls system; in other cases the system connects to the wrong point. Update the units or contact Level 1 support for more assistance. In some cases, Level 1 support may refer you to Level 2 support for further assistance with Enumeration issues.
- Click Action in the top left of the pane.
- Click Create Units and Enum Report.
- Click Save.
- Enter the correct enumeration type for your points in the Excel spreadsheet, if they are not correct.
- Click Points Without or Wrong Units tab at the bottom of the Excel spreadsheet.
- Enter the correct units of measure for your points in the Excel spreadsheet, if they are not correct.
- Click Save.
For more information about units and enumerations, see Enumeration Groups and Supported Units of Measure. Next, you can transfer data between the Professional Productivity Tool and Johnson Controls Enterprise Management.