Applications - Johnson Controls - LIT-1900118 - Electric Actuator - M9106-xGx-2 Series Electric Non-Spring-Return Actuator

M9106-xGx-2 Series Electric Non-Spring-Return Actuators Catalog Page

Product
Document number
LIT-1900118
Revision date
2019-10-09

The M9106 actuators are used to position balancing, control, round, and zone dampers in typical HVAC applications. The M9106 can also be used with an M9000-520 linkage to control 1/2 in. (DN15) to 1-1/2 in. (DN40) VG1000 Series ball valves. The M9106 Series actuator mounts directly on the duct surface, round damper, or small rectangular damper with an anti-rotation bracket and two sheet metal screws (included). Additional linkages or couplers are not required.

Refer to the damper or VAV box manufacturer’s information to select the proper timing for the actuator. Refer to the appropriate application note for specific wiring diagrams and information.

Refer to the M9106-xGx-2 Electric Non-Spring-Return Actuators Product Bulletin (LIT-2681123) or the M9106-xGx-2 Electric Non-Spring-Return Actuators Installation Instructions (Part No. 34-636-1085) for important product application information.