Applications - Johnson Controls - LIT-1900119 - Electric Actuator - M9106-AGx-2N0x Series Electric Non-Spring-Return Actuator

M9106-AGx-2N0x Series Electric Non-Spring-Return Actuators Catalog Page

Product
Document type
Catalog Page
Document number
LIT-1900119
Revision date
2019-10-15

The actuators are used to position balancing, control, round, and zone dampers in typical HVAC applications. They are also used to position the blades in a VAV box. The actuators mount directly to the surface of a VAV box, round damper, or small rectangular damper with a single No. 10 self-drilling sheet metal screw (included). There are no additional linkages or couplers required. Clearly labeled electrical terminals simplify installation. Refer to the damper or VAV box manufacturer’s information to select the proper timing for the actuator.

Note: The damper rotation time must be defined at the controller, and the damper point definition must match the rotation time of the actuator.

When combined with a VAV controller, the actuator provides reliable integrated damper control. Refer to the M9106-AGx-2N0x Series Electric Non-Spring-Return Actuators Application Note (LIT-2681116) for various configurations with and without the DPT-2015 Differential Pressure Transmitter.

Refer to the M9106-AGx-2N0x Electric Non-Spring-Return Actuators Product Bulletin (LIT-2681126) or the M9106-AGx-2N0x Electric Non-Spring-Return Actuators Installation Instructions (Part No. 34-636-1077) for important product application information.