Robust enclosure - Johnson Controls - LIT-12013729 - DP180 - Sensors - DP140 Series Low Differential Pressure Transducer

Low Differential Pressure Transducer DP180 Series Product Bulletin

Product
Switches and Electrical > Differential Pressure Transducers > DP140 Series Low Differential Pressure Transducer
Document number
LIT-12013729
Revision date
2021-05-13
Product status
Active

The DP180 is housed in a NEMA 4 rated housing and is built to withstand harsh environments. The wall mount enables installation of the sensor anywhere to maximize space efficiency in difficult applications.