The Johnson Controls® DP180 Series measure differential or gauge (static) pressure and convert this pressure difference to a proportional high-level analog output for both unidirectional and bidirectional pressure ranges. Every sensor in the DP180 Series is tested and factory-calibrated before shipment. The DP180 Series contains two standard excitation and output versions as shown in Table 1.
Figure 1. DP180 Transducer
Excitation | Output | Output codes |
---|---|---|
9 VDC to 28 VDC | 4 mA to 20 mA | 4 |
9 VAC to 30 VAC 12 VDC to 40 VDC |
0 VDC to 5 VDC | 2 |