All network engine models can integrate to the LonWorks network with the addition of a separate USB-to-LON interface adapter (ACC-USBLON-0). Refer to the SNE/SNC Product Bulletin (LIT-12013296). This required adapter connects the network engine to the LonWorks TP/FT-10 network. The LonWorks network connects to the 3-wire removable, keyed terminal block on the adapter. The SHD connection on the LonWorks network terminal block is an isolated terminal and is not connected in the network engine.
Features | SNE2200x | SNE1100x | SNE1050x | SNE110Lx |
---|---|---|---|---|
LON network variables |
2000 | 1500 | 1500 | N/A |
LON maximum devices |
255 | 127 | 60 | N/A |