SNC - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

All network engine models can integrate to the LonWorks network with the addition of a separate USB-to-LON interface adapter (ACC-USBLON-0). Refer to the SNE/SNC Product Bulletin (LIT-12013296). This required adapter connects the SNC to the LonWorks TP/FT-10 network. The LonWorks network connects to the 3-wire removable, keyed terminal block on the adapter.

Table 1. SNC limits
Features SNC2515x-0 SNC2515x-0H SNC2515x-04 SNC2515x-04H SNC1612x-0 SNC1612x-0H SNC1612x-04 SNC1612x-04H

LON network variables

1500 1500 1500 1500

LON maximum devices

64 4 60 4