Each NAE monitors and controls LonWorks field devices connected to its single LonWorks trunk. The LonWorks FT-10 trunk from the NAE is a single network segment, supporting up to 64 nodes without a repeater. Adding a physical repeater to the trunk allows the NAE to support 127 nodes on a trunk. Depending on the hardware model, the NAE can support up to 255 nodes if LonWorks routers are used on the trunks. Optimum performance is achieved using a maximum of 100 nodes or 1,000 Network Variables (NVs). The NAE supports up to 5,000 total objects, depending on the hardware model.
| Features |
NCE25/NIE29 |
NAE35/NIE39 |
NAE45/NIE49 |
NAE55/NIE59 |
NAE85 |
|---|---|---|---|---|---|
|
LON maximum devices |
32 | 64 | 127 | 255 | N/A |