LCS - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The LCS connects to a ANSI/CTA-852 channel, which runs on a TCP/IP-based network. It supports up to 20 LonWorks IP routers, up to 1,000 total LonWorks devices under those routers, and 10,000 objects total.

Note: The implementation of up to 20 LonWorks IP routers has been tested in a lab environment. However, there are sites that successfully run with more LonWorks IP routers. Run more than 20 LonWorks IP routers at your own risk.
Note: The LCS does not have an IP-70 interface and does not support IP-70 devices.

You can increase the number of objects supported to 25,000 with an LCS license upgrade; however, permanent status item limitations apply after this upgrade. See the LCS permanent status item limitation section. Refer to Software Manager Help (LIT-12012389) for information about how to license software.