Network configuration and device limits - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Configuration and commissioning of the LonWorks trunk is performed using the LonWorks network configuration tool LN-Builder. You may also use a third-party LonWorks network configuration tool, such as the Echelon® LonMaker® tool to configure and commission the LonWorks trunk. See the LonWorks network integration section.