Temporary status items - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Temporary point object polling polls the point as long as Present Value reads continue. This scenario prevents unnecessary polling of points. Whenever Present Value requests for that point are received, the Temporary Status Item Expiration Time period begins. When the Temporary Status Item Expiration Time period expires, all polling for that point stops.

Temporary point object polling is typically used for interval trends.