Temporary Status Item Expiration time - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The Temporary Status Item Expiration Time is the global, user-defined time period for temporary point object polling, applied per individual object. Each time a point object receives a Read Attribute of the Present Value, the Temporary Status Item Expiration Time begins. Polling for the point stops when the Temporary Status Item Expiration Time expires.

Notes:

  • The Temporary Status Item Expiration Time is configured in the Detail view Hardware tab of the LonWorks Integration Object, and defaults to 60 seconds.
  • Changing the Temporary Status Item Expiration Time to a value greater than the trend interval results in nonstop data trending.