Commands - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Integrated LonWorks objects support only those commands that can be executed by a standard LonWorks (LonTalkĀ®) service and network variables. Most Integrated LonWorks objects support commands by writing a value to the network variable. Refer to the Metasys Site Management Portal Help (LIT-1201793) for specific objects and the commands supported in the system.