Trend buffer - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The trend buffer resides on the network engine and provides buffer space for each individual trend. The number of trend samples stored in each individual trend buffer is user configurable. When an individual trend buffer is full, you can configure the trending process to either stop trending or overwrite the older data with the newer data. You can configure an alarm to report whenever the buffer is full and you can also configure the trend buffer to transfer samples to a configured ADS.