LonWorks Field Point object support - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The Metasys system supports network variables of all LonMark SVNTs, all point types in NexSys controllers, and all LN Series Free Programmable Controller internal point types.