Mapping of field values - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Each LonWorks Point Object can be mapped from an LN Series Internal, Network Variable, or NexSys Point object. In the case of Network Variable or NexSys Point, the mapping can be of the whole or a portion of the entity.