Integrated LonWorks objects - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Integrated LonWorks objects represent LonWorks devices and network variables and appear in the Navigation tree. When you select an integrated LonWorks object, the Focus view displays LonWorks parameters in an available panel on the user interface.