Mapped Devices folder - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

A Mapped Devices folder is located under the LonWorks Integration object in the Engineering view. This folder only contains mapped devices and does not show routers because they cannot be mapped.