Diagnostics view - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The Diagnostics view displays LonWorks diagnostic attributes, such as Statistics and Metrics, for troubleshooting purposes. You must send a Latch Statistics command to the LonWorks Integration Object to update these values. Users with high privileges can have access to this view.

Figure 1. Diagnostics view and Permanent Status item count in Metasys UI and Metasys SMP