In addition to the device specific resource files, the LonWorks Integration
object requires the STANDARD.TYP and
STANDARD.FPT resource files, and a
NVConfig.dat file. This NVConfig.dat file is created
automatically, but you need to update it with the correct
configuration data using a network configuration tool, such as
LN-Builder. See Defining a network engine in the LonWorks database.
Note: Once you have created and updated the LonWorks Integration object, add all the resource files
for the LonWorks enabled device types you intend to add to the LonWorks trunk. Adding,
importing device data, or mapping a LonWorks enabled device before loading the resource
files can produce undesired results that may require a reboot.
Note: Network Engines at Metasys
Release 8.1 and earlier are only compatible with STANDARD
resource files at version 13.10. Network Engines at Metasys
Release 9.0 and later are compatible with STANDARD resource
files at version 15.00. You may confirm the version of the
resource file when you open it with a text editor such as
Notepad.