Field device - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The network engine indicates whether the required XIF resource file is present with an attribute called XIF Present. This attribute is located under the Focus and Hardware tabs of the field controller. A value of True indicates that the required XIF resource file is present, and False indicates that the file is missing. If the file is missing, Critical Resource Missing is shown for the status of the device. An alarm message appears when an object without the required XIF file is added to the integration. If any other resource file type is missing, the point object may display Data Conversion Error.

Figure 1. Resource file indication in Metasys UI and Metasys SMP