Resource files - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The LonWorks network integration requires resource files to support integrating LonWorks enabled devices. Device resource files have file extensions of .XIF (External Interface File), .TYP (Type File), and .FPT (Functional Profile Template), and provide device type and configuration data. For example, an LN-VAVLF-1 controller has the following three device specific resource files: LN-VAVLF-1 110.XIF, LNVAVL1.TYP, and LNVAVL1.FPT.

Note: .TYP and .FPT resource files may not be provided for third party devices. In this case, you only need the .XIF file.