LonWorks integration object - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Use the LonWorks Integration object to configure the parameters for LonWorks network integration and its individual LonWorks trunk. Each LonWorks Integration object supports a single LonWorks domain, and only one LonWorks Integration object is allowed per network engine. Refer to the Metasys UI Help (LIT-12011953) or the Metasys Site Management Portal Help (LIT-1201793) for further details on supported objects.