LNS device configuration plug-in - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

LonWorks devices are configured using LN-Builder. For ease of programming, all LN Series, TEC2200, and Flexible System Controller (FSC) devices have plug-ins that allow the user to change device parameters. In addition to changing parameters, the FSC Plug-in allows the user to create an import file that preserves the custom point names that can be imported into the NAE, SNE, or SNC. You can also use the Point Schedule to make changes to points.