LonWorks Point Objects - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product name
LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

LonWorks Point Objects represent point data from a particular LonWorks Device Object. The data is represented as an analog input (AI), analog output (AO), binary input (BI), binary output (BO), multiple input (MI), and multiple output (MO). Generic integration objects (GIOs) can be added via import file only.