Items in the All Items tree in the Metasys SMP UI and the Network tree in Metasys UI - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

You can use LonWorks enabled devices, folders, and NVs that appear as integrated (mapped) objects in the Navigation Tree as object references, allowing the integrated object to be referenced as any other Metasys system object.

The following rules apply when adding integrated LonWorks enabled objects to the Navigation Tree:

  • You must add integrated LonWorks device objects under the LonWorks Integration object.

    Note: You may add devices under a folder as long as the folder resides under the LonWorks Integration object.
  • You must add LonWorks point objects under a LonWorks device object.

  • To group LonWorks point objects within a LonWorks device, add folder (container) objects under the LonWorks device object and add the LonWorks point objects under a folder object.

    Note: See the Object hierarchy section for an illustration of objects in the Navigation Tree.