Device names for auto-discovered devices consist of the device type (extracted from the device's Program ID) and its DNS address, providing a unique identifier for each device (for example, Plant Controller 42 0D 04). The DSN number is used as a unique identifier for each device. Since the DSN number is not a required part of the name, it can be removed if necessary.