Archive database - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The archive database is the Metasys system site database stored, archived by the System Configuration Tool (SCT). The archive database includes the network engine databases for one or more network engines on the site.