This document describes how to perform the tasks required to configure the network engine as a LonWorks network integrator, including how to:
- add a LonWorks Integration object
- insert resource files
- define a network engine on the LonWorks trunk
- map LonWorks enabled devices using Auto Discovery
- map field points in LonWorks devices using Auto Discovery
- map a series of LonWorks enabled devices manually
- map field points in LonWorks enabled field devices manually
- use the Engineering view to view device and point data
- use the Engineering view to command Network Variable Input (NVIs) and NexSys® points
- view detailed router information
- trend LonWorks device data
The Network Automation Engine (NAE) models, SNE series network engines, SNC series network control engines, and LonWorks® Control Server (LCS) with a LonWorks network interface serve as LonWorks network integrators within the Metasys system.
As a LonWorks network integrator, the network engine monitors and supervises LonWorks enabled devices on multiple network segments (or trunks) and is configured as a device on the LonWorks network. Data is presented on a web browser that is logged in to the web-enabled user interface of the engine, or to any other NAE, SNE, SNC, LCS, Application and Data Server (ADS), or Open Application Server (OAS) requesting data over the IP network.