Using the Engineering view to view device and point data - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

About this task

When online with a LonWorks device, you can use the Engineering view of the LonWorks Integration object to view the data of LonWorks devices and points that the network engine has discovered. The Mapped Devices folder contains a list of all mapped devices. The devices and points do not have to be mapped to the Navigation Tree to be acted on.
Note: LN Series internal points are not visible in Engineering View.

To use the Engineering view to view devices and points:

Procedure

  1. Right-click the LonWorks Integration object in the Navigation tree and select View. The LonWorks Integration object appears.
    Figure 1. LonWorks Integration Object (LON Trunk)

  2. Click the Engineering tab and navigate to either a field device or a field point in the Integration Tree.
  3. Double-click the selected field device or field point; the Details screen appears.
  4. Click the x in the upper-right box to close the menu.