Using the Engineering view to command network variable inputs and edit NexSys point data - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

About this task

When online with a LonWorks device, you can use the Engineering view of the LonWorks Integration object to command NVI values for any LonWorks device and to edit NexSys point data. The Mapped Devices folder contains a list of all mapped devices. The NVIs and NexSys points do not have to be mapped to the Navigation Tree to be acted on.

To use the Engineering view to view and edit NVIs and NexSys points:

Procedure

  1. Right-click the LonWorks Integration object in the Navigation tree and select View. The LonWorks Integration object appears.
  2. Click the Engineering tab and navigate to either a field point or NVI in the Integration Tree.
  3. Double-click the selected field point or NVI. The Details screen for the selected field point object or NVI appears.
    Figure 1. Engineering View (Details screen)

  4. Click Edit. The fields that are editable from this screen are shown in a box with a line border.
  5. Make the desired changes, click Save, and close the screen.