Using Auto Discovery - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

LON Point Auto Discovery only allows a defined number of points to be discovered for a single instance. If the total number of discovered points exceeds the limit, then the returned discovery indicates Page 1 of X, where X is the total number of pages. A restart increments the page and displays the next set of discovered points. Each completion of the point mapping process also increments the page. After the last page, the point mapping process begins again at Page 1.

Figure 1. Wizard Auto Detect Utility

Figure 2. Wizard Auto Detect Utility – page increments