Mapping LonWorks Field Devices and Field Points in Metasys UI using Auto Discovery - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

About this task

After you add the LonWorks Integration object and the required resource files, you need to map the devices on the LonWorks network to the network engine.

To map the devices in Metasys UI, complete the following steps:

Procedure

  1. In the Metasys UI, select LON Trunk1 in the Building Network tree.
  2. Click the + icon in the upper left corner of the Building Network tree to add a network item. This displays the Create Item window.
  3. On the General Type dropdown menu, select Field Device and click Discovery.
  4. Search for the device you want to discover in the name column, click Next and then click Create.
  5. Click Add Field Points.
  6. On the General Type dropdown menu, select Field Point and click Discovery.
  7. Select the field point in the name column, click Next and click Create.
  8. To close the Create Item window, click Close.