About this task
You must define the network engine in the LonWorks database to complete the integration process. This defining process creates critical internal bindings and produces a network image of the network engine.
Notes:
- You must define the LCS85 as a device in the IP-852 Configuration Server before you can commission the LCS85 in LNS. See Appendix: Using a Flat LonWorks System with LCS and Appendix: LCS85 Gesytec 852 Configuration Settings for details.
- You must use LN Builder, LonMaker, or LNS Object browser to add a network engine to the system.
To define the network engine on the LonWorks network: