TCP/IP network - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The TCP/IP network provides the transport medium for LonWorks packets according to the ANSI/CTA-852 standard. This standard provides management and encapsulation for the LonWorks packets on the TCP/IP network.

A site may have a single TCP/IP network, but multiple ANSI/CTA-852 channels may be configured within that TCP/IP network.