LonWorks IP routers - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active
LonWorks IP routers allow EIA-709 (LonWorks) packets to travel to and from the TCP/IP network. They are also true LonWorks routers because they must be configured by a LonWorks network management tool to function on the LonWorks network.
Note: If you use an IP852 router that is not manufactured by Echelon Corporation, Loytec, or Adept Systems, it might not be compatible with the LCS85. Refer to the LonWorks Control Server (LCS) 85 Product Bulletin (LIT-12011549) for a complete list of supported ANSI/CTA-852 routers.