Guidelines for network partitioning - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Consider the following when you partition a network:

  • The LNS computer must sit on both networks.

  • Only one Loytec L-IP router can be designated as the Configuration Server for each ANSI/CTA-852 channel.

  • The Loytec L-IP router can be mounted in the server enclosure. As an example, Channel 2 shows a Loytec L-IP router near the LCS85 server at address 10.100.5.1. This router has no nodes attached.

  • The Loytec L-IP router designated Configuration Server may or may not have nodes attached. The device functions primarily as a LonWorks IP router, but has configuration server capabilities. Using it in the field as a router and as the Configuration Server utilizes the full capability of the device.

  • Systems are based on network addresses. Therefore, the logical organization (such as the example in Figure 1) may not match the physical location of the network.

  • The communication in a partitioned system is divided. In the Figure 1 example, the left LCS85 (at address 10.100.5.88) communicates only with Ethernet routers 10.100.5.2, 10.100.5.3, 10.100.5.4, 10.100.5.5, and 10.100.5.6. The right LCS85 communicates only with Ethernet routers 10.100.5.1, 10.100.5.7, 10.100.5.8, 10.100.5.9, and 10.100.5.10. Binding and other data sharing cannot occur between these two systems. Any data sharing between the two groups can only be done with the Metasys system through an Application and Data Server (ADS), or Extended Application and Data Server (ADX).