Network partitioning - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Figure 1 shows a complex system partitioned into two separate LNS databases (2 domains). In this example, devices to the left of center are on Channel 1 (Domain 1), and devices to the right of center are on Channel 2 (Domain 2).

Note: If you are using the Echelon Configuration Server instead of the Loytec Configuration Server, the setup is identical to Figure 1, except that the embedded Configuration Server is disabled on the Loytec L-IP router and the Echelon Configuration Server resides on the LNS Tool (LN-Builder).
Figure 1. Complex System with Partitioned Network