Complex system setup - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

Figure 1 shows a complex system setup with multiple LCS85s operating within the same LNS database (same domain). This setup differs from a basic system because of the additional LCS85 servers.

Note: If you are using the Echelon Configuration Server instead of the Loytec Configuration Server, the setup is identical to Figure 1, except that the embedded Configuration Server is disabled on the Loytec L-IP router and the Echelon Configuration Server resides on the LNS Tool (LN-Builder).
Figure 1. Flat LonWorks Complex System