About this task
This system comprises a single large LNS database containing all nodes in the system with multiple LCS85 servers. The LCS85 servers are segregated to communicate to different devices within the same network. Segregation is based on designating complete FTT-10 channels to each LCS85. You manually partition the system ensuring only specific LonWorks IP routers (or specific nodes) are mapped to the LCS85. No device can be mapped to both systems.
This system closely meets flat LonWorks system specifications and is still considered flat because any node can be bound to any other node in the system. The purpose of LCS85 server segregation is to break up the network into manageable pieces for incorporation into a Metasys system.
Partitioning a network is a way to manage large systems, but does require some caution. Consider the following issues when you partition a large system: