Configure the LonWorks IP routers - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

You need to configure LonWorks IP routers only if you are setting up a new system. If you are working with an existing system, the port number is the only changeable value in the Configuration Server’s related routers.

If this is a new system, the routers need IP addresses. The IP addresses must be static IP addresses, and assigned in cooperation with the IT department to ensure that no current or future conflicts exist.