LNS Turbo or later Edition has an integral 852 communications driver, and can
communicate directly over IP. Driver configuration consists of entering the Ethernet
IP and port address of the Configuration Server.
Important: Removing LNS
TURBO after installation to revert to a previous version of LNS is a manual
process that could result in data loss. Carefully consider this issue if you
choose to install LNS Turbo or later Edition on your computer.