Basic system overview - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

A flat LonWorks System differs from a typical LonWorks network because of its open architecture. This appendix describes the components, setup, and the role of the 852 Configuration Server in a flat LonWorks system organization.