Configure the channels - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

This partitioned system example includes two channels. Table 1 provides the IP addresses of all devices on Channel 1. Table 2 provides the IP addresses of all devices on Channel 2.

Note: If you are using the Echelon Configuration Server instead of the Loytec Configuration Server, the channel configuration is identical to what is shown in Table 1 and Table 2, except that the embedded Configuration Server is disabled on the Loytec L-IP router. Additionally, the Echelon Configuration Server resides on the LNS Tool (LN-Builder) and is configured to handle two separate LNS networks. The defined Configuration Server uses the same IP address with a unique port number in each instance to segregate the separate LNS networks.
Table 1. Channel 1 IP Addresses

IP Address

Device

10.100.5.2

Loytec L-IP Router Configuration Server

10.100.5.3

Loytec L-IP Router

10.100.5.4

LonWorks Ethernet Router

10.100.5.5

Loytec L-IP Router

10.100.5.6

Loytec L-IP Router

10.100.5.88

LCS85 Server

10.100.5.200

LNS Computer

Table 2. Channel 2 IP Addresses

IP Address

Device

10.100.5.1

Loytec L-IP Router Configuration Server

10.100.5.7

LonWorks Ethernet Router

10.100.5.8

LonWorks Ethernet Router

10.100.5.9

LonWorks Ethernet Router

10.100.5.10

LonWorks Ethernet Router

10.100.5.99

LCS Server

10.100.5.200

LNS Computer