Configure the LNS computer - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Product
Integrations > Lonworks Integrations > LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active

The LNS computer has particular requirements for configuration during setup. Setup must be carefully considered, as each configuration option has its own effects on the system. See the Basic system overview section for information on ANSI/CTA-852 driver issues.

Setting up two LNS Computers is the equivalent to having two basic systems. Each LonWorks system is independent and set up separately. Both systems are simple, but the complete setup requires more hardware and software.