Troubleshooting communication between the configuration server and devices - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Brand
Johnson Controls
Product name
LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active
Language
English
  • Reset the router so the router table gets updated correctly. The router does not pass data across channels if the router tables are not correct.
  • Check the configuration settings of the router if communication cannot be established by the configuration server. Make sure the settings match those specified in this appendix.
  • Establish the connection between a device and the configuration server by selecting the device in the LonWorks Interfaces list and clicking Test.
  • Use the Update Members command for the Echelon Configuration Server, or use the Recontact command for the Loytec Configuration Server if any devices are not communicating.
  • Check your firewall and antivirus settings if communication cannot be established with any of the defined devices. Disable the firewall and antivirus software if necessary for testing.